Wanting to add wireless charging receiver to project. Scared of ruining the board by putting it in the wrong place. Battery obviously is linked to battery pads, but where do I connect the receiver? Someone said the “USB-C connector” on the board, but I am worried about connecting to wrong place and ruining the board (I know they are cheap, but I don’t want to if I can just ask). Thanks in advance for help.
Hi there,
It’s a fair question, You can use something like this device:
https://www.amazon.com/Dpofirs-Wireless-Charging-Receiver-Interface/dp/B0B5M15V5S
HTH
GL
PJ ![]()
FYI, You be powering the Xiao with the USB-C connection and recharging the Battery connected to the battery pads I would surmise? If so very inefficient , Try a power bank with a solar panel instead.
It’s a small wearable device. I have this that I was going to use: Amazon.com
The device will be enclosed in a case. Was hoping to not have any large external openings on the case.
Hi there,
Yes I have seen those and I think I even have one, “300ma” may not be enough or large’ish input capacitor for the Xiao Startup Gulp or power.
Some testing and power profiler would be required.
HTH
GL
PJ ![]()