Accidentally "Boot-Looped" my SenseCAP Solar Node P1 Pro

OK I TRIED your zip file and a similar named file from meshtastic flasher and i still got boot loop.. what da?

the incorrect firmware overwrote important flash partitions happened here, so the normal startup fails shortly after Bluetooth initialization. When the wrong Meshtastic/Rak UF2 image is pushed to the Solar Node, then it happens.

Enter the DFU mode (double-tap reset so you see the “XIAO-BOOT” drive)> use a flash erase UF2 (It will wipe the flash before loading the correct firmware)>re-flash the proper bootloader (if needed)>he correct Meshtastic application UF2. you should follow this Get Started with SenseCAP Solar Node | Seeed Studio Wiki?

1 Like

Hi there,

Yes, It took a couple tries to get it clean , before the Flasher would write a good image, once it did , everything was per the Wiki, AOK!
GPS is working Also. :+1:

HTH
GL :slight_smile: PJ :v:

Hey folks, first post. Seeed Solar node has a solid transmit light in the meshtastic app and is transmitting packets constantly. Tried to reflash the firmware but it fails repeatedly. I’m assuming I need to flash the boot loader as described above? BT connection works for awhile and then drops for some reason. Lights on the unit seem to be working normally.