Hi there. From the pin-out diagram of Xiao-esp32c3 I can see that it has SPI pins. I have Groove Vision AI v2 and an attached Xiao-esp32c3. I would like to know if it is possible to access the SD card by esp32c3 in the attached Groove Vision AI v2 through SPI? from the schematic diagram i can see esp32-c3 connector MISO/MOSI connection to HX6538, but not the SD card.
All varients of ESP32 I have tried allow you to assign the SPI pins, SCK, MOSI, MOSI to most all available GPIOs.
The program cores might well have defaults applied for the SPI pins, and these might be shown on the pin maps, but you normally can change them.
Hi, thanks. I figured out from documents that Xiao can sent AT command to Groove vision AI 2 to save and access images in SD card, but there is no direct link with Xiao to the SD card module in Groove Vision AI 2.
Regards.
Could you share how to access the images on the SD card with AT commands?
Hi there,
and Welcome,
From what I gleen is , You use the Xiao Serial port to receive your AT command from the keyboard. That is passed to the Sccm one the Himax chip and “IT” reads or writes the Jpeg to the TF card. Here is the protocol guide from the WiKi
HTHT
GL
PJ
Hi and thanks for your reply! I understand how to write images to the SD card, but I do not understand how to read images from the Groove Vision AI v2 SD using AT commands on the Xiao board. I do not yet have Groove Vision AI v2 to test but would be glad if @rmukhia could share how he did it.
Sorry, I was not able to solve my problem of reading the saved image. After going through the AT command, documentation and source code. I can see that there is no support to read images from SD card through uart AT command. SSCMA-Micro firmware which runs in the Groove Vision 2 does not support it, from what I understand.
On a side note, if you interested in just the image feed AI.last_image() might help.
Hi Seeed Team and Community,
I recently purchased the Grove - Vision AI Module V2 (Arm Cortex-M55 & Ethos-U55) and unfortunately, the micro SD card holder (9+4 pin short body) on the board got damaged during use.
Could you please help me with the following:
- Exact part number or model of the micro SD card holder used on the board.
- Recommended source or supplier (Digikey, Mouser, LCSC, etc.) where I can order a replacement.
Hi there,
And Welcome Here…
SO, I looked at the unit I have and I see it looks very similar to the one installed on the ROUND display. The Schematic for that is on the WIKI so the part number may be there as well, if the BOM viewer is there maybe it would help too.
If nothing else , then a BUMP for Seeedineers ![]()
HTH
GL
PJ ![]()
Hello,
I’m currently using the XIAO ESP32C3, and I’ve been advised to connect its interface and update the firmware to ensure proper operation.
However, I’m not sure how to proceed, and I might be facing a driver or firmware issue.
Could anyone help me resolve this problem?
Hello, you can refer to the wiki document to get some assistance.
That’s an interesting setup. From what I understand, the key question is whether the Grove Vision AI module exposes the SD card to the attached XIAO ESP32C3 or keeps it managed internally. I’d start by checking the module documentation and any example projects to see how storage access is implemented. If you’ve already tested communication between the two devices, sharing your current approach might help others suggest a more specific solution.