Accessing Arduino from the installed WIN10 OS

I have purchased the Odyssey - X86J4105*64. I want to program the Arduino Co-Processor to obtain Sensor Data through the GPIO. I want to program the GUI Interface using WIN10 installed on the Odyssey.

I cant find any references on how to do this as it keeps referring to the Arduino using Linux running Ubuntu. I dont have Linux, I have the installed WIN10.

I sincerely hope I can do this task, or at least access the 40-pin header from within WIN10. I really need some direction here, than you everybody.

Paul

@BasicBasic please refer this thread How do I connect to the Arduino CPU from within the Odyssey X86 Mini PC