Hi,
Hope that all of you are doing well.
I would like to access to ssh of senseCAP M2 gateway to install tailscale VPN.
Could you please show me how?
Thank you in advance for your reply.
Best regards.
i dont think there is a raspberry pi inside
Hi there,
Pretty sure anything with a SSH can be an endpoint. YMMV
basic VPN from end to end without a config file. is what I understand.
HTH
GL
PJ
![]()
I like SoftEther VPN , have several businesses using it , nicely with drobo’s and freenas.
RDP works perfectly. but i digress
i tried and it denied the connection… its running openwrt if that helps
Hmm, did you use root? no password
PJ ![]()
How do I access SSH on OpenWrt?
Linux terminal emulators
- Open a terminal emulator and write ssh [email protected] (“ssh” is the command, “root” is the OpenWrt user you are connecting to, and “192.168.1.1” is OpenWrt default IP )
- there will be a message about accepting a new key from the OpenWrt device, write “yes” and press Enter key.
out of the box experience , BTW.
or check this one out.
https://openwrt.org/docs/guide-quick-start/sshadministration
Microsoft Windows [Version 10.0.19045.4529]
(c) Microsoft Corporation. All rights reserved.
C:\Users\cgwal>ssh [email protected]
ssh: connect to host 192.168.1.111 port 22: Connection refused
C:\Users\cgwal>
Looks like the Inn is Closed today… Probably has it’s own Pword.
LOL
PJ ![]()