hello
We use reTerminal to connect the QR reader to the USB port
The voltage may drop when operating the QR reader. QR reader maximum power consumption is 400mA
ReTerminal recognizes that a single USB port can supply 500mA of power.
Is it correct as an action? Also, is there any countermeasure for supplying a stable voltage?
nengyu
January 13, 2023, 2:38am
2
You could try buying a hub with USB power
Hi nengyu
thanks for the reply
We will also consider the USB powered hub you suggested.
By the way, is it difficult to stably operate a 400mA device from reTerminal’s USB port as a specification?
nengyu
January 13, 2023, 3:03am
4
If the USB2.0 protocol standard is followed, the power supply current is about 500mA, but due to circuitry and its own losses, it may cause instability.
Thanks for the reply
We will try to ensure sufficient voltage and current.