About the “SenseCraft” Category

Welcome to the hub for the SenseCraft software ecosystem :star_struck: . Use this space to discuss topics on publishing AI applications, designing physical data interfaces, and managing IoT networks.

1 Like

salve

perche quando scollego la xiao esp32 S3 dal pc, dopo aver installato firmware, non funziona piu?

My E1001 stopped updating the Google Calendar Widget yesterday. I am getting a 504 error when connecting to Tools on the SenseCraft website. The website shows the updated calendar information, and the reTerminal is connected to the internet. Are Seed Studio servers having an issue?

1 Like

Hi There,
Probably one of the most Asked and un explained questions of Seeed Studio cc

SenseCraft “What is it …” ?

SenseCraft (hosted at sensecraft.seeed.cc) serves as Seeed Studio’s all-in-one web portal and ecosystem for edge AI, IoT device management, and no-code application building.

Seeed Studio

It acts as an umbrella platform containing several web-based portals and tools:

  • SenseCraft AI: A web console for exploring over 400 pre-trained vision, sound, and anomaly detection models, training custom models, and deploying them to edge devices like the XIAO ESP32S3 Sense or Grove Vision AI modules with a single click.

    SenseCraft - Seeed Studio

  • SenseCraft Data Platform: Formerly known as the SenseCAP Portal, this is their IoT cloud backend used for gateway/node onboarding, telemetry monitoring, and managing sensor data.

    sensecap.seeed.cc

  • SenseCraft HMI / Seeedash: A web-based, drag-and-drop visual interface builder designed to configure dashboards and e-paper displays (like those used with reTerminal or desktop e-ink boards) without writing code.

    Seeed Studio

  • CodeCraft & Web Toolkits: Browser-based development tools that allow you to generate code, configure parameters, flash firmware, and manage devices directly through WebSerial from a browser window.

    GitHub

Think of SenseCraft as the “app store” and control panel for Seeed’s smart devices.

If you’re someone who is new to technology:

Imagine you buy a smart security camera or a temperature sensor, but it doesn’t come with any pre-installed software. Instead of writing complicated computer code from scratch to make it work, you go to SenseCraft in your web browser.

It’s a website where you can look at a catalog of ready-made ‘brains’—like a program that recognizes faces, detects sounds, or tracks data—and install them onto your device with just one click. You can also use it to view charts of what your sensors are doing or change your device’s settings visually, without needing to know anything about programming.

In the most simple terms…

HTH
GL :slight_smile: PJ :v:

I would wager We will see more of these and this SAS (Software as a Service)
it allows some level of proprietary bridge to using Opensource code in your own products and not disclosing the modifications. Which we all no is NOT open source spirit. It is What it is, And LOL :grin: won’t belong until someone if they haven’t already REA’d it, Will no avoiding it.