About the General category

When there is no other category, General is the way to go :wink:

I have been noticing the number of Replies compared to the number of Views.
There are many Views but very few Replies (in relation to).
There is a message in those numbers.
Unfortunately the message is not good for Seeed customers.
Yes, they like it when you buy their products, but please don’t expect any real support.
I think I made a big mistake buying the Seeed ReSpeaker 4-mic array and an even bigger mistake when I renewed my subscription to Hack Space magazine (where I first encountered the ReSpeaker).

2 Likes

hello/ Order Number : 210515152000 still not recived. I wait 5 month already. Tracking number that you provided not valid

1 Like

Absolutely,
I have sent countless (at least 5 emails) to various email accounts on their website, some bounced, no one replied. I purchased the product, and realised its not very good for my intended purpose, and yet the only offer is to join this forum - for what? No support? This company sux and ill be keen to avoid and share my dislike if ever i get the chance to. Pure waste of money and crap company to go with it!

1 Like

I might be being really stupid here, but how does one go about posting a new topic ?

I can’t see how that is done at all.

Thanks

2 Likes

I had the same question. According to Seeed Technical Support, you start a level 0, and need to browse Seeed forums until you get promoted to level 1.
Once you reach level 1, you will be able to post a topic. That’s the “basic” badge:
“Thanks for sticking around and reading a few topics to learn what our community is about. New user restrictions have been lifted; you’ve been granted all essential community abilities, such as personal messaging, flagging, wiki editing, and the ability to post multiple images and links.”
You will then see a new button “+New Topic”

1 Like

The whole point of a forum is usually to help with issues. I can’t even post to ask for help, seems silly… you should at least have a beginner category for new people to at least ask simple seed questions until they are able to post elsewhere. I came here to ask a question to see if your hardware would work for my product idea prior to purchasing a bunch of them. If I can’t even get any kind of pre-sales community interaction, that seems sketchy no?

2 Likes

Me too. I’m just wandering around the forum aimlessly and replying here and there (like now !) just to work off my time or replies or reads or whatever the hell they are counting in the hope that I can soon ask a question.

2 Likes

I am also here posting in the hopes that I will be able to ask my beginner question soon :frowning:

I have selected the XIAO ESP32S3 for a project and just need to know if I can use serial over USB, and also use the pins labeled Tx and Rx for GPIO at the same time.

The getting started page is helpful, but not clear on this detail.

1 Like

Reply points!

I found this on one of the messages. Seems we need to be Trust Level 1:

Get to trust level 1 by…

  • Entering at least 5 topics
  • Reading at least 30 posts
  • Spend a total of 10 minutes reading posts
3 Likes

Ah thanks, that’s good to know. I think I’ve replied 3 or 4 times to posts so nearly there !

1 Like

I’m trying to get an original V1.0 Respeaker unit going and I’ve got issues following the instructions, results didn’t match the expected ones, so I want to reset everything but can’t get rid of the “overlay” sd card file system thing.

1 Like

Are there also forums where one can ask a question? I registrered because I wanted to ask a question, but there doesn’t appear to be such a function for new members? Amateur hour.

1 Like

I am still waiting do be “promoted” to question-asking privileges !

I’ve read a good few posts and posted half a dozen times but still no “Ask a question” or “New topic” button for me either.

1 Like

!!! I’ve been promoted !!! This very morning, the sun is shining as well ! Things are looking great !

Still no “new topic” button though…

I couldnt find the best place to post this, but why can I not create a new topic if I have a question?

Hi there,

And Welcome here…

It’s an Anti Spam thing, you need to reply to a few posts and then you’ll have all the normal capabilities.

HTH
GL :slight_smile: PJ :v:

Hi PJ Glasso,

Thanks for inviting me to the forum. I was hoping to get some specific help with a single nRF52840 board that seemingly cannot connect to anything via bluetooth. However, this anti-spam thing seems to prevent me from posting any new topics. Like several of the other users above, I don’t have that privilege at the time of commenting.

Are there instructions somewhere that show more clearly how and when the promotion happens? Is it a waiting period thing? Do I need to leave a certain number of comments? Do I need to follow a certain number of topics?

Thanks

Hi there,

and Welcome here.

just reply to this again , I think it takes 3 , then you get enough forum credz to post links, etc. They got bombed bad a while back so it’s a PITA but needed so.,bare with it, After it’s no issues.

What was the BLE issue? you were having ? I have a drag and drop file in the drag&Drop thread to test that has some BLE demo code running you can connect to the Xiao with Mobile or Desktop using NRF connect for each (desktop) needs $9 dongle. but does a ton of other stuff too, if your troubleshooting or working with BLE projects must have IMHO.

HTH
GL :slight_smile: PJ :v:

1 Like

Hi PJ_Glasso, Thanks for inviting me to follow up here. Sorry about the delay, I got busy with life. I’m back.

My device is running firmware that was programmed by a well respected member of a community that makes video game controllers.

The firmware is hosted on Github. I guess because of user permissions I cannot include any hyperlinks in my post but it is in jfedor2’s repository called “slimbox-bt”

My board design is a simple breakout. I made it to use commonly available arcade stick wiring harnesses to hook the board up to arcade joysticks and buttons for more comfortable living room play. I am “CapnHawke” on Github. The board designs are visible in my “Game controller parts” repo.

I ordered boards from JLCPCB. Because they have a minimum order quantity of five, I ended up with a bunch of extra breakouts. In early April, I soldered on my first xiao nRF52840 (Controller #1). The board successfully took firmware and I started playing video games with it.

The expected behavior is as follows:

  • The controller appears to my PC as a “Flatbox rev 7” controller. It uses the same drivers as a google stadia controller.
  • After pressing and holding the “start” button for three seconds, it enters pairing mode, and is visible in a list of bluetooth devices. I can also see the device on my iPhone.
  • After attempting to pair the device on my PC, it should connect and immediately start functioning as a gamepad.
  • Button presses register in joy.cpl on Windows devices.

Reasoning that I had a bunch of breakout boards left over, I ordered three more xiao nRF52840 boards and batteries in late June or early July, and attempted to make three additional controllers. I struggled to get firmware on all of them, but at this point I am ready to chalk it up to simple user error. I did eventually get firmware on all three of these (controllers numbered 2, 3, and 4). Controller #2 and #3 both work fine, though I still need to wire them up to actual joysticks and buttons.

Controller #4 has problems with a bluetooth connection. Although Controllers #2 and #3 both follow the expected behavior outlined above, Controller #4 gets stuck at the bluetooth pairing step. It is visible to my PC as a Flatbox Rev 7, just as expected, so there is definitely not a problem with the transmitter on the board. However, when I choose it as a device to pair with, the bluetooth connection instantly fails. The timing is very consistent. The device disappears momentarily from the list of available bluetooth devices while pairing is being attempted, and after the bluetooth connection fails, it reappears as a new device with the same name in my bluetooth devices list. If I do this over and over, I can get my list of bluetooth devices to populate with multiple “Flatbox rev 7” devices, all of which (except for the most recent instance) have failed to connect.

That is where things stand currently. I’m at a bit of a loss on where to go from here. I won’t rule out that it might have been a bad board from the start. I did not test the board before soldering it to a breakout. But I might have also damaged it with clumsy soldering work. I am unsure.