Hello,
I checked the device log using UART, and it seems that it’s failing due to the Jetson overheating. I don’t have a fan installed. Is that usually required just to flash?
Here is the end of the log:
[ 9.685504] NET: Registered PF_INET6 protocol family
[ 9.686311] Segment Routing with IPv6
[ 9.68631ib/8] ules/5.15.14In-8-tu Oegr(IO wia/uth IPvpdates/drivers/nvpps/n
insmod /lib/modules/5.15.148-tegra/updates/drivers/net/ethernet/nvidia/nvethern
insmod /lib/modules/5.15.148-tegra/kernel/drivers/usb/typec/stusb160x.ko
insmod /lib/modules/5.15.148-tegra/updates/drivers/platform/tegra/mce/tegra-mce
insmod /lib/modules/5.15.148-tegra/updates/drivers/spi/spi-tegra210-quad.ko
[ 9.726715] tegra-qspi 3270000.spi: Adding to iommu group 8
[ 9.727273] tegra-qspi 3270000.spi: Prod config not found for QSPI: -19
[ 9.728763] spi-nor spi0.0: mx25u51279g (65536 Kbytes)
[ 10.745319] using random self ethernet address
[ 10.745324] using random host ethernet address
[ 10.760372] tegra-xusb 3610000.usb: Firmware timestamp: 2023-02-10 03:48:10 C
[ 10.915631] usb0: HOST MAC 66:b9:ae:4f:7b:74
[ 10.915634] usb0: MAC 46:47:6b:41:d1:53
[ 10.915653] tegra-xudc 3550000.usb: EP 0 (type: ctrl, dir: out) enabled
bash: cannot set terminal process group (-1): Inappropriate ioctl for device
bash: no job control in this shell
bash-5.1# [ 11.363000] tegra-xudc 3550000.usb: EP 5 (type: intr, dir: in) enad
[ 11.363018] tegra-xudc 3550000.usb: EP 3 (type: bulk, dir: in) enabled
[ 11.363030] tegra-xudc 3550000.usb: EP 2 (type: bulk, dir: out) enabled
[ 11.363115] IPv6: ADDRCONF(NETDEV_CHANGE): usb0: link becomes ready
[ 63.732860] EXT4-fs (nvme0n1p1): mounted filesystem with ordered data mode. .
[ 154.789932] thermal thermal_zone0: cpu-thermal: critical temperature reachedn
[ 154.790303] reboot: HARDWARE PROTECTION shutdown (Temperature too high)
[ 154.798680] reboot: Failed to start orderly shutdown: forcing the issue
[ 154.798953] kvm: exiting hardware virtualization
[ 155.123067] arm-smmu 12000000.iommu: disabling translation
[ 155.127914] arm-smmu 8000000.iommu: disabling translation
[ 155.132560] tegra-mc 2c00000.memory-controller: unknown: read @0x00000000000)
[ 155.133231] tegra-mc 2c00000.memory-controller: unknown: read @0x00000000000)
[ 155.134038] reboot: Power down
����Shutdown state requested 0
Shutting down system …