- Does the M.2 Key M supports PCIe or only SATA? I am trying to see if I can use it for something other than an SSD for my M.2 card which is also Key M but PCIe.
- Can the M.2 Key E be used with an M.2 Key M using an Key E to Key M adapter cable?
Hi, the A203 board supports PCIE, but SATA can also be connected to the PCIE port via an adapter cable.
As for the second question, I think it should not work, because some pins are empty pins and there should be no such conversion line.
Are you able to use the M.2 key M slot to pick up an nvme ssd?
I have been attempting to so and cannot figure out how to.
Hello everyone,
Have any update about this issue ?
I’m also using A203v2 attached a Xavier NX and a Samsung NVMe SSD in the M2 Key M Connector.
Although the NVMe SSD is shown when I typed the command: ‘lspci’, but it is not shown up in ‘lsblk’ command.
My Xavier NX + NVMe SSD can work in Nvidia Xavier NX Developer Kit normally.
Have any problems with my A203v2 Carrier board ?
Please help me ! Thank you very much !
Best Regards,
Dat Phung
Hello, did you install the driver before using the A203 carrier board?