The “DSONanoQuadExportFileReader” is a cool idea, but I think I’ll continue to develop BenfWaves for the time being. It’s in C#, it’s source-controlled and has a repository and revision history both visible on the internet, it’s reasonably well-documented, it automatically generates API documentation with Doxygen, uses annotated-class System.Xml.Serialization, uses sane Windows Forms binding, can support multiple open documents using MDI, and is built with expandability in mind. I’ll continue to add conversion formats, and eventually I’ll work on adding a waveform viewer, perhaps integrating gnuplot or some other open-source graphing library so that it can be anti-aliased and easily navigable. I’d love to get together some beta testers to start marking down bugs and feature requests, but that isn’t really urgent.