A client for BenF's DSO Nano XML

Hello Folks,

Sorry for the delay but I have had work commitments that I had to complete before getting back to my hobby project.

Ok so here we have the first beta release of the DSO nano XML export file reader. This version features the following.

• XML import

• Trace reproduction with the ability to set the time and signal levels.

• Scroll through the sample

• Zoom to Max/Min signal values and zoom to trigger point.

• Signal offset

• Trigger level marker

• Export to CSV, TSV, Excel, Matlab

• Ability to save screen view as screen sot to file

• Ability to save and load configuration settings including last loaded file

• Auto time and level scaling according to the XML profile parameters

• FFT signal representation for both LOG and amplitude

• Ability to select trace colours for both time and frequency representation of data

• Splash Screen on start up

• About screen with version number

For future proofing when the QUAD comes on line and an XML export is available for that I have also started on a logic analyser that will decode UART and I2C signals.

Screen shots show what it looks like and a ZIP of the EXE is also here for download.

Any suggestions on design or functionality welcome.

Cheers Pete


DSONanoXMLExportFileReader.zip (127 KB)