Hi, I have a 5G card from Quectel RM500Q-GL (the most popular one everyone is using ) in the Odyssey. I run ubuntu 20.10 with modem manager 1.14.2. and I see that it is by default connected on the data interface with USB 2.0
sherlock@dt-minion-1:~$ sudo lsusb -D /dev/bus/usb/001/007
Device: ID 2c7c:0800 Quectel Wireless Solutions Co., Ltd.
Device Descriptor:
bLength 18
bDescriptorType 1
bcdUSB 2.10
bDeviceClass 0
bDeviceSubClass 0
bDeviceProtocol 0
bMaxPacketSize0 64
idVendor 0x2c7c Quectel Wireless Solutions Co., Ltd.
idProduct 0x0800
bcdDevice 4.14
iManufacturer 1 Quectel
iProduct 2 RM500Q-GL
This will be limiting on the 5G network with wide 80-100 MHz channel that should hit close to 1Gbps
Does anyone knows how to set that card to USB 3 Superspeed or native PCI-E mode?
It looks it should be supported. Does Odyssey suports USB3 on that M.2 connector?
wSpeedsSupported 0x000f
Device can operate at Low Speed (1Mbps)
Device can operate at Full Speed (12Mbps)
Device can operate at High Speed (480Mbps)
Device can operate at SuperSpeed (5Gbps)
bFunctionalitySupport 1
Lowest fully-functional device speed is Full Speed (12Mbps)
bU1DevExitLat 1 micro seconds
bU2DevExitLat 500 micro seconds
SuperSpeedPlus USB Device Capability:
bLength 20
bDescriptorType 16
bDevCapabilityType 10
bmAttributes 0x00000001
Sublink Speed Attribute count 1
Sublink Speed ID count 0
wFunctionalitySupport 0x1100
bmSublinkSpeedAttr[0] 0x000a4030
Speed Attribute ID: 0 10Gb/s Symmetric RX SuperSpeedPlus
bmSublinkSpeedAttr[1] 0x000a40b0
Speed Attribute ID: 0 10Gb/s Symmetric TX SuperSpeedPlus