Can you please advice me how to increase the range for 433Mhz RF link kit (SKU: WLS107B4B / seeedstudio.com/depot/433mhz … th=139_140).
Currently I have no more than 5 meters range (with 20 cm antenna on both sender and receiver and 5V supply) and very low concrete wall penetration; this is very low compared with a 433 Mhz wireless weather station (that works well thru concrete wall on a 10 meters range and is powered with 3V on the TX side and 5V on the RX side).
For the last several days I investigated this issue with different TX units (weather sensors, RF remote controls) and I suspect there is some improvement to be done on the RX side. I already tried to increase the power voltage from 5 to 12V.