2oz/70uM Cu?

is there any way to get boards made with 2oz/70uM Copper instead of 1oz/35uM?

How many boards do you need?
our fusion PCB just can produce the 1oz Cu.

Thanks
Albert

I was going to produce 10-20 atm. I will do calculations to verify if 1oz will hold up.

Thanks for the response
Bob

For prototypes, try soldering some copper wire (or solder wick) along areas that must carry high current. If you do this, it’s advisable to modify the design so there is no soldermask in the areas you want to run this copper wire.