Hi there, I just download the respeaker-debian-9-lxqt-sd-20180801-4gb.img.xz and use the etcher to burn it to board, it works. Here is the screen output. Actually, we do verify the firmware previously. do you see any error during etcher burning process? If no, please download the image once again and test. please do let us know if the issue is still there. thanks.
Debian GNU/Linux 9 v2 ttyGS0
respeaker.io Debian Image 20180801
Support/FAQ: http://respeaker.io
default username:password is [respeaker:respeaker]
v2 login:
Bill