2 Temp&Humi Sensors on the same Arduino

Hey Rony,

Thank you so so much!

I was stuck on getting some response while using the analogue inputs :smiley:

I just tested 2 and while they are next to each other, they output totally different results. I also let them settle for about 15 minutes before copying the results you see below.

Read sensor 1: OK
Humidity1 (%): 37.00
Temperature1 (oC): 22.00
Read sensor 2: OK
Humidity2 (%): 33.000
Temperature2 (oC): 21.000

Humidity is off by 4% and Temperature by 1oC. :frowning:

It says there on the wiki page that:

(see http://www.seeedstudio.com/wiki/Grove-_Temperature_and_Humidity_Sensor)

…but reality hit me pretty hard :cry: