Hey guys,
I am trying to use 2 Temperature & Humidity Sensor Modules (http://www.seeedstudio.com/wiki/Grove-_Temperature_and_Humidity_Sensor) with the same Arduino. As the code for using only one sensor is quite complicated for my skill level, I would really need some help.
Thank you so much,
zws
[code]#define DHT11_PIN 0 // ADC0
byte read_dht11_dat()
{
byte i = 0;
byte result=0;
for(i=0; i< 8; i++){
while(!(PINC & _BV(DHT11_PIN))); // wait for 50us
delayMicroseconds(30);
if(PINC & _BV(DHT11_PIN))
result |=(1<<(7-i));
while((PINC & _BV(DHT11_PIN))); // wait '1' finish
}
return result;
}
void setup()
{
DDRC |= _BV(DHT11_PIN);
PORTC |= _BV(DHT11_PIN);
Serial.begin(9600);
Serial.println(“Ready”);
}
void loop()
{
byte dht11_dat[5];
byte dht11_in;
byte i;
// start condition
// 1. pull-down i/o pin from 18ms
PORTC &= ~_BV(DHT11_PIN);
delay(18);
PORTC |= _BV(DHT11_PIN);
delayMicroseconds(40);
DDRC &= ~_BV(DHT11_PIN);
delayMicroseconds(40);
dht11_in = PINC & _BV(DHT11_PIN);
if(dht11_in){
Serial.println(“dht11 start condition 1 not met”);
return;
}
delayMicroseconds(80);
dht11_in = PINC & _BV(DHT11_PIN);
if(!dht11_in){
Serial.println(“dht11 start condition 2 not met”);
return;
}
delayMicroseconds(80);
// now ready for data reception
for (i=0; i<5; i++)
dht11_dat[i] = read_dht11_dat();
DDRC |= _BV(DHT11_PIN);
PORTC |= _BV(DHT11_PIN);
byte dht11_check_sum = dht11_dat[0]+dht11_dat[1]+dht11_dat[2]+dht11_dat[3];
// check check_sum
if(dht11_dat[4]!= dht11_check_sum)
{
Serial.println(“DHT11 checksum error”);
}
Serial.print(“Current humdity = “);
Serial.print(dht11_dat[0], DEC);
Serial.print(”.”);
Serial.print(dht11_dat[1], DEC);
Serial.print("% ");
Serial.print(“temperature = “);
Serial.print(dht11_dat[2], DEC);
Serial.print(”.”);
Serial.print(dht11_dat[3], DEC);
Serial.println("C ");
delay(2000);
}[/code]