It also looks like I’m having problems installing the libraries in the Arduino folder. I load them where they belong, but they do not show up ater restarting the program. I have renamed other folders from touchscreen to touchscreen2 and touchscreenlibrarymaster and rename them to just touchscreen when I want to use them, but renaming touchscreenlibrarymaster to touchscreen and opening the Arduino program, it does not show up?
I have removed the other folders named touchscreen… and left the touchscreenlibrarymaster as touchscreen. It shows up but still does not work. Also tried another but it wants a file called stdint.h. I can’t find that anywhere…