2.8'' TFT Touch Shield - TFT BMP demo problem!

Hello there. I also have issues with the 2.8’’ TFT Touch Shield. I am using it with SD card shield and Arduino uno. I copied the two 24-bit bmp pictures in a SD card and getting the exact picture like seppala_timo. I tried to uploaded but I got a message from this forum: “Your post looks too spamy for a new user, please remove off-site URLs.”

Here the code I am using. I only changed the default pin (53) to 10.

// This sketch is adapted to Seeed’s TFT library by ladyada/adafruit under MIT license

#include <SD.h>
#include <TFT.h>

// In the SD card, place 24 bit color BMP files (be sure they are 24-bit!)
// the file itself
File bmpFile;

// information we extract about the bitmap file
int bmpWidth, bmpHeight;
uint8_t bmpDepth, bmpImageoffset;

void setup()
{
Serial.begin(9600);

Tft.init();

Serial.print(“Initializing SD card…”);
pinMode(10, OUTPUT); //53 is used as chip select pin

if (!SD.begin(10)) { //53 is used as chip select pin
Serial.println(“failed!”);
return;
}
Serial.println(“SD OK!”);

}

void loop()
{
Tft.setOrientation(0);

//Image 1
bmpFile = SD.open(“flower.bmp”);
if (! bmpFile) {
Serial.println(“didnt find image”);
while (1);
}

if (! bmpReadHeader(bmpFile)) {
Serial.println(“bad bmp”);
return;
}

Serial.print("image size “);
Serial.print(bmpWidth, DEC);
Serial.print(”, ");
Serial.println(bmpHeight, DEC);
bmpdraw(bmpFile, 0, 0);
delay(3000);
bmpFile.close();

//Image 2
bmpFile = SD.open(“hibiscus.bmp”);
if (! bmpFile) {
Serial.println(“didnt find image”);
while (1);
}

if (! bmpReadHeader(bmpFile)) {
Serial.println(“bad bmp”);
return;
}

Serial.print("image size “);
Serial.print(bmpWidth, DEC);
Serial.print(”, ");
Serial.println(bmpHeight, DEC);
bmpdraw(bmpFile, 0, 0);
delay(3000);
}

/*********************************************/
// This procedure reads a bitmap and draws it to the screen
// its sped up by reading many pixels worth of data at a time
// instead of just one pixel at a time. increading the buffer takes
// more RAM but makes the drawing a little faster. 20 pixels’ worth
// is probably a good place

#define BUFFPIXEL 20

void bmpdraw(File f, int x, int y) {
bmpFile.seek(bmpImageoffset);

uint32_t time = millis();
uint16_t p;
uint8_t g, b;
int i, j;

uint8_t sdbuffer[3 * BUFFPIXEL]; // 3 * pixels to buffer
uint8_t buffidx = 3*BUFFPIXEL;

for (i=0; i< bmpHeight; i++) {

  Tft.setXY(x, y+bmpHeight-i); 


for (j=0; j<bmpWidth; j++) {
  // read more pixels
  if (buffidx >= 3*BUFFPIXEL) {
    bmpFile.read(sdbuffer, 3*BUFFPIXEL);
    buffidx = 0;
  }
  
  // convert pixel from 888 to 565
  b = sdbuffer[buffidx++];     // blue
  g = sdbuffer[buffidx++];     // green
  p = sdbuffer[buffidx++];     // red
  
  p >>= 3;
  p <<= 6;
  
  g >>= 2;
  p |= g;
  p <<= 5;
  
  b >>= 3;
  p |= b;
 
   // write out the 16 bits of color
  Tft.sendData(p);
}

}
Serial.print(millis() - time, DEC);
Serial.println(" ms");
}

boolean bmpReadHeader(File f) {
// read header
uint32_t tmp;

if (read16(f) != 0x4D42) {
// magic bytes missing
return false;
}

// read file size
tmp = read32(f);
Serial.print(“size 0x”); Serial.println(tmp, HEX);

// read and ignore creator bytes
read32(f);

bmpImageoffset = read32(f);
Serial.print("offset "); Serial.println(bmpImageoffset, DEC);

// read DIB header
tmp = read32(f);
Serial.print("header size "); Serial.println(tmp, DEC);
bmpWidth = read32(f);
bmpHeight = read32(f);

if (read16(f) != 1)
return false;

bmpDepth = read16(f);
Serial.print("bitdepth "); Serial.println(bmpDepth, DEC);

if (read32(f) != 0) {
// compression not supported!
return false;
}

Serial.print("compression "); Serial.println(tmp, DEC);

return true;
}

/*********************************************/
// These read data from the SD card file and convert them to big endian
// (the data is stored in little endian format!)

// LITTLE ENDIAN!
uint16_t read16(File f) {
uint16_t d;
uint8_t b;
b = f.read();
d = f.read();
d <<= 8;
d |= b;
return d;
}

// LITTLE ENDIAN!
uint32_t read32(File f) {
uint32_t d;
uint16_t b;

b = read16(f);
d = read16(f);
d <<= 16;
d |= b;
return d;
}

And here the serial output log:

[quote]
Initializing SD card…SD OK!
size 0x38436
offset 54
header size 40
bitdepth 24
compression 40
image size 240, 320
2169 ms
size 0x38436
offset 54
header size 40
bitdepth 24
compression 40
image size 240, 320
2171 ms
size 0x38436
offset 54
header size 40
bitdepth 24
compression 40
image size 240, 320
2170 ms
size 0x38436
offset 54
header size 40
bitdepth 24
compression 40
image size 240, 320
2171 ms
size 0x38436
offset 54
header size 40
bitdepth 24
compression 40
image size 240, 320
2170 ms

Any help with this matter it would be highly appreciate. Thanks in advance.