I can not for some reason seem to get the 2.8" TFT touch screen, the SD Shield, and the ardunio uno all to work together. I seem to be unable to load images from the SD card. From the what I’ve been able to figure out it seems that the screen can’t load images at the same time as they are being retrieved from the card. It makes a sort of static garbage that doesn’t seem to ever load an image. Does anyone have a script that actually works so I can build off of it? So far not even the scripts included on the wiki don’t work. If I have confirmation that a script someone else has works I can narrow down the possible issues. I do not have a script as an example because I have no idea where to start and the premade scripts do not work. I need something that does work so I can learn how to make something. Any assistance would be appreciated. Thanks in advance.
Hi.Maybe you can refer to this topic:http://www.seeedstudio.com/forum/viewtopic.php?f=23&t=4150