I bought recently the 125Khz RFID reader (UART version) but it seems it is broken.
I already tried/observed:
I can see (with a jyetech scope) a 125Khz signal on ant1 en ant2 connections. This is distorted when a card is nearby (tried multiple cards, all the same behaviour), so I think the tags and RF circuit/Antenna are working.
I also looked at the rx/tx pin with this scope, but I only see some garbage during startup and then pulled to Vcc. But no changes in voltage (i.e. no digital signal) when a card is present or not, swiped etc.
I did check that, but there is no digital activity when the unit is powered and a card is presented to the reader (and moved away) it is just pulled to Vcc.
I think the mcu has no firmware or the mcu is broken… Is there a firmware upgrade procedure that I can try? or need to place a jumper or send an init string?
I am sorry that you cannot upgrade the firmware yourself.
to confirm the MCU is not working , you can test the winding connector by a oscillograph , if you can not see the 125K square wave output from circuit , that the module must be broken.