Hello,
I’m using the component: http://wiki.seeedstudio.com/Grove-125KHz_RFID_Reader/
I have build a program using Python with raspberry zero to read the RFID tag number and everything is working fine. I was just wondering how I can boost the reading distance. Can I push up the input voltage? Can I set a parameter? Do I need to build a new antenna?
I would like a reading distance of 8 cm, but now I must push the badge against the antenna to get a read.
Thank you,
best regards,
Sander
Hi Sander,
You can change to 51*82 antenna to extend the ranger. But we do not sale the antenna separately. How many quantity do you need? thanks.

Bill
Hello, I only need 1 antenna.
Can you confirm that this antenna gives a reading distance of 70mm?
thank you,
best regards
Hi there, it shall be able to. But we do not sale antenna this moment. thanks.
Bill