I received my : “125Khz RFID module - UART” yesterday in the mail.
I have it connected to an Arduino UNO, exactly how the photos are shown on the WIKI.
I am running the sample code from the WIKI.
The LED on ‘P3’ - is always on. It’s on with an antenna, without an antenna. ?
the serial output from the unit via the Arduino interface shows no data ever?
I’m speculating that their is something wrong with the hardware?
Glad to know that you are interested in this module. The LED port is always HIGH , it will be LOW only if at the moment that a 125kHz RFID card be read by RFID module. If it is always HIGH , only two possibilities , either the RFID Card is not work with this module , or there is something wrong with its hardware.
Hi~ we are not the designer of this RFID module , just distribute it. While , as what we know , this module is work with some 125k RFID cards include the card sold in our store. We can not make sure that this module can read all of the 125k RFID card, because different card has different features such as some card with security protection.