How to use the WIO I2C port for connecting the Soil Moisture (Capacitive Sensor)?

I want to connect two Grove Soil Moisture sensor to one WIO terminal.

Connecting one to the Analog port works, how do I connect the other one to the I2C port ( the one near to the power button)?

The two 4-Pin interfaces provided by Wio Termianl are a Grove interface and the other is an IIC interface. If the Grove interface is occupied, it is recommended that you use the row holes on the back of Wio Termianl to connect.

Thank you, I did that, and it worked.