CAM and DRU Files for Eagle?

Moderators: lily.li, violet, carmen.zheng

Post Reply
gion
Pre-kindergarten
Pre-kindergarten
Posts: 9
Joined: Mon Apr 30, 2018 1:20 am

CAM and DRU Files for Eagle?

Post by gion » Thu Dec 27, 2018 5:10 am

Hello,
I can't find the link to download the .dru and .cam profile for Eagle. Could anyone provide me a link?
I'm using an old version Eagle, so I don't have Seeed rules provided with the program...

Thank you

carmen.zheng
Staff
Staff
Posts: 94
Joined: Wed Apr 04, 2018 3:41 pm
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: PCB, PCBA, PCB Layout, 3D Printing, CNC Milling and more!
Location: Shenzhen
Contact:

Re: CAM and DRU Files for Eagle?

Post by carmen.zheng » Thu Dec 27, 2018 8:10 pm

Hi Gion,

The old CAM files are still on the How to Generate Gerber files from Eagle page. The DRC was taken down but I have included them both here.

A few notes first, I recommend that you update to the latest Eagle version and use the built-in CAM files since they do resolve a few problems that were present in the past. I can't remember the details but generally it is better.

CAM files
http://www.seeedstudio.com/document/rar ... -layer.zip
http://www.seeedstudio.com/document/rar ... -15-16.rar

Similarly, for the DRU files, they were taken down since they caused customers some confusion. For example, the minimum drill hole diameter is 0.3mm but actually you can have 0.2mm drill holes, they just cost extra. So, is that a DRU violation or not? It depends on the customer's budget.

DRU files (use with caution)
http://www.seeedstudio.com/document/rar ... 140221.rar
http://www.seeedstudio.com/document/rar ... 140221.rar

Post Reply