(TECH) Unable to falsh Adrunio IDE firmware
Moderators: lily.li, violet, jessie, chao.zhang
(TECH) Unable to falsh Adrunio IDE firmware
Hi,
I have been trying to flash my unit with the firmware for the Arduino IDE. I am following the instructions on the Wiki (http://www.seeedstudio.com/wiki/Arduino ... or_RePhone).
1. I have powered off the unit
2. Started the flasher (called Updatefirmware.exe in the instructions but is called FirmwareUpdater.exe in the download zip file)
3. Click the download button
4. Connect the unit to the USB port
5. I wait, but no download starts and eventually (about 20 to 30 seconds later I get a slow blink of the green light)
6. After 1 minute I get a timout message
I am using Windows 7 Pro 64 bit, on an Alienware laptop.
Please advise how to proceed and get the firmware in place.
thanks
Carl
I have been trying to flash my unit with the firmware for the Arduino IDE. I am following the instructions on the Wiki (http://www.seeedstudio.com/wiki/Arduino ... or_RePhone).
1. I have powered off the unit
2. Started the flasher (called Updatefirmware.exe in the instructions but is called FirmwareUpdater.exe in the download zip file)
3. Click the download button
4. Connect the unit to the USB port
5. I wait, but no download starts and eventually (about 20 to 30 seconds later I get a slow blink of the green light)
6. After 1 minute I get a timout message
I am using Windows 7 Pro 64 bit, on an Alienware laptop.
Please advise how to proceed and get the firmware in place.
thanks
Carl
Last edited by carl19 on Sat Jan 30, 2016 1:13 am, edited 1 time in total.
Re: Unable to falsh Adrunio IDE firmware
usb disconnect
rebootshort - no led
firmwareupdater start
choose rephone
klick download
usb connect
if you see flash drive - wrong
if you see com ports - right
thats all
usb disconnect
usb connect
if you see flash drive - drive is empty
now you can upload : RePhone Create Kit VXP
or a aduino sketch
or eclipse ...
rebootshort - no led
firmwareupdater start
choose rephone
klick download
usb connect
if you see flash drive - wrong
if you see com ports - right
thats all
usb disconnect
usb connect
if you see flash drive - drive is empty
now you can upload : RePhone Create Kit VXP
or a aduino sketch
or eclipse ...
Re: Unable to falsh Adrunio IDE firmware
Thanks for the reply, none of those processes have worked for me.
So I decided to try with another machine. I tried another 64 bit windows machine but no joy. I did finally succeed in updating my firmware with an old Windows XP SP2 32 bit machine.
Once it was updated everything seems to be okay.
Carl
So I decided to try with another machine. I tried another 64 bit windows machine but no joy. I did finally succeed in updating my firmware with an old Windows XP SP2 32 bit machine.
Once it was updated everything seems to be okay.
Carl
Re: (TECH) Unable to falsh Adrunio IDE firmware
my os
windows 10 32-bit
on dell laptop
maybe you habe problems with the
mtk usb debug port and
mtk usb modem port ?
the install program do not work on my system
i must install over device manager and
manual call the inf file
over
append legacy hardware
and choose the inf file with the explorer
windows 10 32-bit
on dell laptop
maybe you habe problems with the
mtk usb debug port and
mtk usb modem port ?
the install program do not work on my system
i must install over device manager and
manual call the inf file
over
append legacy hardware
and choose the inf file with the explorer
Re: (TECH) Unable to falsh Adrunio IDE firmware
I had the same problem but after several trials an errors now it works - no reason why.
Maybe these advices help to avoid or overcome the problem:
- install the drivers as admin.
- be shure, that the battery has enough power.
- run "\Arduino_IDE_for_RePhone-master\drivers\mtk\UninstallDriver.exe" to repair driver issues.
Good luck!
Maybe these advices help to avoid or overcome the problem:
- install the drivers as admin.
- be shure, that the battery has enough power.
- run "\Arduino_IDE_for_RePhone-master\drivers\mtk\UninstallDriver.exe" to repair driver issues.
Good luck!
-
- Pre-kindergarten
- Posts: 22
- Joined: Tue Feb 02, 2016 6:18 am
Re: (TECH) Unable to falsh Adrunio IDE firmware
Hello.
I'm in the same situation as the OP. Can't get firmware to flash though. Any ideas?
Hardware appears to working properly. Home screen etc.
Followed driver installation directions step by step.
FirmwareUpdater times out. I've tried and re-tried multiple times.
I'm running Win 7 64bit as admin.
Would anyone who has been successful at updating firmware be kind enough to confirm something for me?
When the RePhone is off(solid red LED) and usb connected the device shows up in device manager under "Network Adapters" as "Alcatel Single RNDIS Interface" and driver details shows two driver files in Windows\system32\drivers\....sys.
When the Rephone is on(blinking Green LED) and usb connected the device shows up in device manager under "Ports" as "MTK USB Debug Port(COM14)" and "MTK USB Modem Port(Com13).
Is this what you are seeing in your system? I'm trying to troubleshoot what might be holding the firmware update process up and not sure what the cause is.
I've also uninstalled and reinstalled the drivers multiple times to no avail.
Thank you for reading.
I'm in the same situation as the OP. Can't get firmware to flash though. Any ideas?
Hardware appears to working properly. Home screen etc.
Followed driver installation directions step by step.
FirmwareUpdater times out. I've tried and re-tried multiple times.
I'm running Win 7 64bit as admin.
Would anyone who has been successful at updating firmware be kind enough to confirm something for me?
When the RePhone is off(solid red LED) and usb connected the device shows up in device manager under "Network Adapters" as "Alcatel Single RNDIS Interface" and driver details shows two driver files in Windows\system32\drivers\....sys.
When the Rephone is on(blinking Green LED) and usb connected the device shows up in device manager under "Ports" as "MTK USB Debug Port(COM14)" and "MTK USB Modem Port(Com13).
Is this what you are seeing in your system? I'm trying to troubleshoot what might be holding the firmware update process up and not sure what the cause is.
I've also uninstalled and reinstalled the drivers multiple times to no avail.
Thank you for reading.
-
- Pre-kindergarten
- Posts: 22
- Joined: Tue Feb 02, 2016 6:18 am
Re: (TECH) Unable to falsh Adrunio IDE firmware
Any updates from Seeedstudio on a possible cause for this issue or troubleshooting tips that I can try?
I have two RePhone kits and neither of them will accept a firmware update.
Followed the Arduino IDE tutorial and the Eclipse tutorial to no avail.
In both cases the FirmwareUpdater times out showing no progress.
Not sure if this helps diagnose the problem, but occasionally I get this debug error...
Thank you for reading.
I have two RePhone kits and neither of them will accept a firmware update.
Followed the Arduino IDE tutorial and the Eclipse tutorial to no avail.
In both cases the FirmwareUpdater times out showing no progress.
Not sure if this helps diagnose the problem, but occasionally I get this debug error...
Thank you for reading.
FirmwareUpdater
Assembly Version: 1.0.0.0
Win32 Version: 1.0.0.0
CodeBase: file:///C:/RePhone/Arduino_IDE_for_RePhone-master/hardware/tools/mtk/FirmwareUpdater.exe
----------------------------------------
System.Windows.Forms
Assembly Version: 2.0.0.0
Win32 Version: 2.0.50727.5491 (Win7SP1GDR.050727-5400)
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System.Windows.Forms/2.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
----------------------------------------
System
Assembly Version: 2.0.0.0
Win32 Version: 2.0.50727.5485 (Win7SP1GDR.050727-5400)
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System/2.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
System.Drawing
Assembly Version: 2.0.0.0
Win32 Version: 2.0.50727.5495 (Win7SP1GDR.050727-5400)
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System.Drawing/2.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
----------------------------------------
System.Core
Assembly Version: 3.5.0.0
Win32 Version: 3.5.30729.5420 built by: Win7SP1
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System.Core/3.5.0.0__b77a5c561934e089/System.Core.dll
----------------------------------------
************** JIT Debugging **************
To enable just-in-time (JIT) debugging, the .config file for this
application or computer (machine.config) must have the
jitDebugging value set in the system.windows.forms section.
The application must also be compiled with debugging
enabled.
For example:
<configuration>
<system.windows.forms jitDebugging="true" />
</configuration>
When JIT debugging is enabled, any unhandled exception
will be sent to the JIT debugger registered on the computer
rather than be handled by this dialog box.
- chao.zhang
- Kindergarten
- Posts: 81
- Joined: Thu Jan 22, 2015 9:55 am
Re: (TECH) Unable to falsh Adrunio IDE firmware
Hi bconstructive,bconstructive wrote:Any updates from Seeedstudio on a possible cause for this issue or troubleshooting tips that I can try?
I have two RePhone kits and neither of them will accept a firmware update.
Followed the Arduino IDE tutorial and the Eclipse tutorial to no avail.
In both cases the FirmwareUpdater times out showing no progress.
Not sure if this helps diagnose the problem, but occasionally I get this debug error...
Thank you for reading.
FirmwareUpdater
Assembly Version: 1.0.0.0
Win32 Version: 1.0.0.0
CodeBase: file:///C:/RePhone/Arduino_IDE_for_RePhone-master/hardware/tools/mtk/FirmwareUpdater.exe
----------------------------------------
System.Windows.Forms
Assembly Version: 2.0.0.0
Win32 Version: 2.0.50727.5491 (Win7SP1GDR.050727-5400)
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System.Windows.Forms/2.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
----------------------------------------
System
Assembly Version: 2.0.0.0
Win32 Version: 2.0.50727.5485 (Win7SP1GDR.050727-5400)
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System/2.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
System.Drawing
Assembly Version: 2.0.0.0
Win32 Version: 2.0.50727.5495 (Win7SP1GDR.050727-5400)
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System.Drawing/2.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
----------------------------------------
System.Core
Assembly Version: 3.5.0.0
Win32 Version: 3.5.30729.5420 built by: Win7SP1
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System.Core/3.5.0.0__b77a5c561934e089/System.Core.dll
----------------------------------------
************** JIT Debugging **************
To enable just-in-time (JIT) debugging, the .config file for this
application or computer (machine.config) must have the
jitDebugging value set in the system.windows.forms section.
The application must also be compiled with debugging
enabled.
For example:
<configuration>
<system.windows.forms jitDebugging="true" />
</configuration>
When JIT debugging is enabled, any unhandled exception
will be sent to the JIT debugger registered on the computer
rather than be handled by this dialog box.
Just now we've tried flash the firmware on different operation systems, say win10, win8, win7, win XP, and it all works fine.
We will keep testing and work it out for you.
BTW could you please try this, after successfully installed the driver, connect the Xadow GSM+BLE to computer without the battery connected, then check if you were able to see a COM PORT named 'MTK USB Port' , which keeps jumping out and gone in the device manager. This is the port used to flash the firmware.

Best regards,
Chao Zhang
-
- Pre-kindergarten
- Posts: 22
- Joined: Tue Feb 02, 2016 6:18 am
Re: (TECH) Unable to falsh Adrunio IDE firmware
Thank you for replying Chao. I got the FirmwareUpdater to work! It turns out that in my case(Window7 64bit) I needed to manually install the drivers and use the "usb2ser_Win764.inf" file. Now the Rephone works fine and is programmable through the Arduino IDE as well.
It's a bit embarrassing that I didn't see that note in the tutorial regarding Windows 7 sooner. Perhaps you might consider increasing the font size on that line in case other people run into the same issue. You also could include it in a troubleshooting guide if you have one going.
Thanks again for getting back to me. Now I'm off to have some fun with my new RePhone
It's a bit embarrassing that I didn't see that note in the tutorial regarding Windows 7 sooner. Perhaps you might consider increasing the font size on that line in case other people run into the same issue. You also could include it in a troubleshooting guide if you have one going.
Thanks again for getting back to me. Now I'm off to have some fun with my new RePhone

- chao.zhang
- Kindergarten
- Posts: 81
- Joined: Thu Jan 22, 2015 9:55 am
Re: (TECH) Unable to falsh Adrunio IDE firmware
Hi bconstructive,bconstructive wrote:Thank you for replying Chao. I got the FirmwareUpdater to work! It turns out that in my case(Window7 64bit) I needed to manually install the drivers and use the "usb2ser_Win764.inf" file. Now the Rephone works fine and is programmable through the Arduino IDE as well.
It's a bit embarrassing that I didn't see that note in the tutorial regarding Windows 7 sooner. Perhaps you might consider increasing the font size on that line in case other people run into the same issue. You also could include it in a troubleshooting guide if you have one going.
Thanks again for getting back to me. Now I'm off to have some fun with my new RePhone
Thanks for the feedback, I will find a way to highlight those keywords

Cheers.