I found HEX binaries in root directory of archive, but if I tried to install any of them (i suppose there are three version to three different slots), no one is possible to install. Each try seems to be succesfull (fast unmount/mount and rename HEX to RDY extension) but nothing on DSO is overwritten. There is still previous one version of DSO active in slot1 and previously installed LOGIC analyzer in slot 3.
May be I missed something, or included HEX is wronlgy compiled a recompilation necessary. I want to start building of development environment for future improvement participation, but now I need to use DSO with best actual FW…
Thank you very much Wildcat. You fixed the triggering so now I can see occasional bursts of data on a serial line. This scope hase been practically useless to me until now.
You moved DSO Quad form almost unusable toy to quite nice DSO. I hope that we get soon merged FW of yours and Pmos’s version with good buttons layout - each FW i tried used different mapping and for me it was necessary to print help card with buttons mapping. (I see Wildcat buttons mapping to be most effective - especially moving some fucntion from jogdials to big buttons is nice.
May be let discuss some definitive buttons functions layout and keep it across future versions…
I was very disappointed by severity and amount of bugs in official firmware as very poor and incomplete doc.
So it is necessary strongly recommend to newcomers IMMEDIATELY switch to PMOS or WILDCAT version!!!
However per the last picture posted here, it’s really a sub set of green CH4. This buggered me for a while. Long press of play/pause doesn’t seem to do anything.
I’ve been using the Wildcat version as my main app which functions very nicely as a scope.
I can’t seem to make sense of the signal generator part though. It sets the waveform and the amplitude OK but all the frequencies seem to be off by a factor of 4. E.g. when I set 1KHz I get a 250 microsecond period waveform on the display rather than the 1msec I was expecting. The timebase looks OK against normal external signals.
There is something like a bug and is a kind of mirror behavior in realtime scan with short buffer
Other Small thing is that the Square that tells the size of the buffer (bottom middle) only fills complete if the full screnn is off, when full screen is activated the scan looses almost 4 squares of measurement. Thank you
Triggered by a comment in another post, I figured out that Wildcat needs the standard SYS rather than the modified SYS25116 I had been using on the community edition. I put Sys1.52 on and now the signal generator frequencies match the display.
I have two of these and they’re really great. First came with Sys version 1.51 and App version 2.52. The second was bought this year and came with Sys version 1.51 and “App (plus A1) Version 1.00”, of which more later. I have flashed your V1.24 APP_G251.hex, which is much better than the 2.52, with some great features and bug fixes. Note that I’ve left it on SYS 1.51 for now and it seems to work except spectrum analyser. I’d like to try Wildcat’s version for comparison, which is why I left 1.51 sys, but I can’t seem to get it to work: I upload the three .HEX files, appx.hex, then renamed to app_0001.hex, then renamed to APP_0001.HEX, then loaded on with power cycle in-between files, but all I get is the boot screen with the buzzer stuck on. What am I doing wrong?