Hello
I don’t understand the behaviour of Pedro’s FFT.
I use a 10kHz “sine” from the internal DAC, channel A with 0.5V/div, 100uS/div as an example.
[list]
Maybe this has to do with the fact that only 256 samples are used, i.e. only about 10 periods and this is not enough - does the FFT only give good results when there is an integer number of periods in the 256 samples? Could this explain why the sines have so many harmonics?
I had another problem, which looks like a bug: when moving the “navigator B”, changing between the “trigger” and the “auto/norm…” menus - but not changing anything at the settings - sometimes the FFT result change completely!!!
Two more questions:
[list]
Patrick