Start Google Assistant from Code

Hello,



Just received my respeaker and ready to start exploring now. What I would like to achieve is the following scenario:


  1. Connect a sensor to the respeaker (say temperature)
  2. Read the data
  3. Check If the temperature > 25 degrees celcius
  4. If so, start a Google Assistant Skill, that says the temperature is very high.



    I’m sure that with some efforts I can get the first 3 to work. Im trying to figure out the last part, and whether it’s even possible at all.

    To clarify, I would like to have the google assistant talk without saying the wake work, without being asked. Any help would be appreciated. I would also be fine with a (good) hack.