Help Required - HTTP Posting- Wio GPS Board- GSP and Temperatur to a Client

Simplify IoT Development.

Moderators: lily.li, violet, seth.welday

Post Reply
markus.schmeckenbecher
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Sat Jan 11, 2020 2:44 am

Help Required - HTTP Posting- Wio GPS Board- GSP and Temperatur to a Client

Post by markus.schmeckenbecher » Sat Jan 11, 2020 3:15 am

Hi Guy,

Im from Germany and need some help. Im bought a "Wio GPS Board" to built up a tracking Solution. Now I figured that not all Arduino Library are being supported by seeed especially not TiniGSM is not supported with the onboard MC20 Modem.

I need the board to built up a simple tracking solution with GSPs and Temperatur which should be sent to ThingsBoard Cloud.

This Cloud support JSON API for the telemetry upload like this with a "Access_TOKEN-ID" to publish telemetry data.
The stated that the format should look like this.

http(s)://host:port/api/v1/$ACCESS_TOKEN/telemetry
{"key1":"value1", "key2":"value2"}

Has someone an idea or reference coding how this can be realized with the Wio to sent HTTP Posting?


Markus

User avatar
salmanfarisvp
Elementary-1
Elementary-1
Posts: 177
Joined: Sun May 20, 2018 2:02 am
Are you a staff member of seeedstudio?: no
Which products/projects are your favorite?: Linklt One , BeagleBone Green , ReSpaker
Contact:

Re: Help Required - HTTP Posting- Wio GPS Board- GSP and Temperatur to a Client

Post by salmanfarisvp » Sun Jan 12, 2020 12:56 pm

Hi,

Which development board are you using? Wio Tracker or something else?
Thank You :) .


Post Reply