(IDEA) A DIY phone to save your children, dog, family, pets,

Moderators: lily.li, violet, jessie, chao.zhang

Post Reply
ortega.fernando
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Wed Jan 13, 2016 4:29 pm

(IDEA) A DIY phone to save your children, dog, family, pets,

Post by ortega.fernando » Fri Jan 15, 2016 5:16 am

I want to show you my project. I think it is something that everyone has thought.

When we are at a party or a place with many people, sporting event, beach, celebrations, etc. we are always afraid of our children are lost. There are today some tracking system sold but they are only bluetooth devices with a little and usefulness range of 10 meters.

The system I am proposing is a DIY phone system that has both GPRS and GPS.

Taking advantage of the modular system that offers us SEEED, you will DIY a small phone with GPRS, a GPS module and a battery.

The operation will be as follows:

Option 1. With GPRS to send data. The system continuously uploads to a website the GPS location. The interval in minutes could be programmed by sending an SMS to the same module. Apart from the GPS position data, it could also upload the battery status, temperature, and so on

Option 2. GPRS not necessary. Only after receipt of an SMS with a certain code, uploads to the website the GPS position data, battery, and so on..

To save space and energy, it could be dispensed without GPRS module and function only via SMS, so that the system will answer an incoming SMS message with the requested data by sending a SMS.

Logically, phone numbers previously authorized to send such SMS would be configured, discarding any SMS from other numbers.

It can be installed in a shoe. It would have just to expose a micro USB connection to charge the battery.

However, the system can be installed in hanging neck, bracelets, backpacks double bottom, and so on.

The GPS position allows a infinite range, because, despite our efforts, the child could be lost or hijacked (for this reason it is hide in the sole, double bottom of a backpack, and so on), GPS position It will give us valuable information to get our children back.

It could be also used with dogs, pets, grandparents, ...

I hope you like this idea !!!! Thank you.

adam+seeed
Pre-kindergarten
Pre-kindergarten
Posts: 23
Joined: Sat Dec 05, 2015 8:43 am

Re: (IDEA) A DIY phone to save your children, dog, family, p

Post by adam+seeed » Fri Jan 15, 2016 10:47 am

:ugeek:

That's similar to one of the ideas I was going to try: a "Weasley Clock" implemented with GSM+BLE, displayed on a clock in the house.
----------
Keyboard for RePhone SMS messages:
Forum Thread: http://www.seeedstudio.com/forum/viewto ... 18&p=24134
GitHub Code: https://github.com/scriven42/RePhone_Cr ... ource_Code

Post Reply