2 Channel CAN BUS FD Shield for Raspberry Pi - Error Experienced

Applications/questions using Raspberry Pi with Seeed products, please post it here.

Moderators: lily.li, salmanfarisvp, violet

Post Reply
chris.letter.box
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Sep 16, 2019 10:31 am

2 Channel CAN BUS FD Shield for Raspberry Pi - Error Experienced

Post by chris.letter.box » Tue Nov 19, 2019 8:19 am

Hi,

I have a Seeed CAN BUS Card and have installed it on top of a Sixfab Pi 3G-4G/LTE Base Shield V2 which is using USB cable for comms.
I havent wired the CAN card up yet to a CAN circuit but ran the install procedures on Seeed website.
Then got this on dmesg | grep spi

[ 5.201525] mcp25xxfd spi0.0: MCP2517 successfully initialized.
[ 5.226249] mcp25xxfd spi1.0: MCP2517 successfully initialized.
[ 5049.919314] mcp25xxfd spi0.0 can0: CAN Bus error experienced
[ 5049.920374] mcp25xxfd spi0.0 can0: CAN Bus error experienced
[ 5375.909019] mcp25xxfd spi0.0 can0: CAN Bus error experienced
[ 5375.909960] mcp25xxfd spi0.0 can0: CAN Bus error experienced

Got this msg from ip -details link show can0

4: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 72 qdisc pfifo_fast state UP mode DEFAULT group default qlen 65536
link/can promiscuity 0 minmtu 0 maxmtu 0
can <LISTEN-ONLY,BERR-REPORTING,FD> state ERROR-PASSIVE (berr-counter tx 128 rx 0) restart-ms 1000
bitrate 500000 sample-point 0.875
tq 25 prop-seg 34 phase-seg1 35 phase-seg2 10 sjw 1
mcp25xxfd: tseg1 2..256 tseg2 1..128 sjw 1..128 brp 1..256 brp-inc 1
dbitrate 8000000 dsample-point 0.600
dtq 25 dprop-seg 1 dphase-seg1 1 dphase-seg2 2 dsjw 1
mcp25xxfd: dtseg1 1..32 dtseg2 1..16 dsjw 1..16 dbrp 1..256 dbrp-inc 1
clock 40000000numtxqueues 1 numrxqueues 1 gso_max_size 65536 gso_max_segs 65535

Can anyone suggest what might be happening ?
Do I need to wire to a CAN circuit first or ?

Thanks

Chris

Post Reply