I just bought the Raspberry Pi Relay Board v1.0 and I was told that it could output 24 Volts DC

Hi,
I just bought the Raspberry Pi Relay Board v1.0 and I was told that it could output 24 Volts DC .
I need to connect my raspberry pi to a mist maker that takes 24 Volts. So the solution was to use this relay.
My question is how do I specify the output of 24 Volts ?

Thanks

Hi there,


The relay is HLS8L-DC5V-S-C. You can refer to

https://datasheet.octopart.com/HLS8L-DC5V-S-C-Helishun-datasheet-43200959.pdf.


The Max output is 30VDC. So it supports 24vdc.

Thanks

best rgds
Bill