CAN-BUS Shield V2 - two SD card

Hi,



I have a problem with the CAN-BUS Shield V2.0 extension,

when I add a second card, it doesn’t detect my first one.

I’m testing a two card project from the SDFat library.



error: cardBegin failed

SD errorCode: 0X20,0XFF



Card error on CAN shield,

What could be the reason for the problems?

Arduino Mega

CS PIN CAN - 9 (default)

CS PIN SD1 - 4 (default)

CS PIN SD2 = 53

Hi There

Can you show me your physical photo? :oops:

i assume you got two CAN-BUS Shield V2 on arduino .

For hardware,Select anyone ,Cut the wire between pad4 and the middle pad. and Weld the middle pad and pad 5.

ps: visit <LINK_TEXT text=“http://wiki.seeedstudio.com/CAN-BUS_Shi#resources”>http://wiki.seeedstudio.com/CAN-BUS_Shield_V2.0/#resources</LINK_TEXT> to view detail

For software,CS PIN SD1 - 4 (default) ,CS PIN SD2 = 5

:smiley: