@PJ_Glasso
Here in attchment my full design, it have many things bca I’m doing a preliminary testing about the module.
Here an example of the output when the module is connected by a central device (I’m using an Android phone and the nRF Connect app installed through the Play Store)
INFO BLE: RSSI = -58
Acc: 0.191;0.849;0.469
Gyr: 1.050;-2.870;0.210
Temp: 26.82
AnIn0: 1633.081
DS18B20 #0: 28.438
leds are blinking at different rate as specified into the source code.
Next step is to set tx power to +8dbm, do you have some suggest?
Thanks and best regards!
Fire
xiao_nrf52840_test.zip (3,6 KB)