XIAO store data in QSPI flash memory

In order to make sure the new library works, make sure that the file structure inside the library folder you are adding to your Arduino IDE master library looks similar to this. May need to go several layers deep in the folder until you see similar to this:

Then either drop in the new folder (unzipped) in the Arduino master library (restart Arduino IDE); or import it with the ZIP function from the IDE menu (make sure it is zipped).