XIAO Sense nRF52840 LittleFS on QSPI Flash with FreeRTOS

Hi there,
You can look at the Speed test and Diags with the Adafruit Flash examples
Writing and testing Both QSPI flash and External “grove flash”
Instantiate them both for Littfs or as SD card. The Adafruit examples do Work with minimum tweaks.
HTH
GL :slight_smile: PJ
see how they read and write, erase…

/*
  ----------------------------------------------------------------------------------------------------------------------------------
  |                                                            Winbond Flash                                                         |
  |                                                      SPIMemory library test v3.0.1                                                |
  |----------------------------------------------------------------------------------------------------------------------------------|
  |                                                                Marzogh                                                           |
  |                                                              16.11.2016                                                          |
  |                                                          Modified: hanyazou                                                      |
  |                                                              19.11.2017                                                          |
  |----------------------------------------------------------------------------------------------------------------------------------|
  |                                     (Please make sure your Serial monitor is set to 'No Line Ending')                            |
  |                                     *****************************************************************                            |
  |                                                                                                                                  |
  |                     # Please pick from the following commands and type the command number into the Serial console #              |
  |    For example - to write a byte of data, you would have to use the write_byte function - so type '3' into the serial console.   |
  |                                                    --------------------------------                                              |
  |                                                                                                                                  |
  |  1. getID                                                                                                                        |
  |   '1' gets the JEDEC ID of the chip                                                                                              |
  |                                                                                                                                  |
  |  2. writeByte [address] [byte]                                                                                                   |
  |   '2' followed by '2435' and then by '224' writes the byte 224 to address 2435                                                   |
  |                                                                                                                                  |
  |  3. readByte [address]                                                                                                           |
  |   '3' followed by '2435' returns the byte from address '2435'                                                                    |
  |                                                                                                                                  |
  |  4. writeWord [address] [word]                                                                                                   |
  |   '4' followed by '5948' and then by '633' writes the int 633 to address 5948                                                    |
  |                                                                                                                                  |
  |  5. readWord [address]                                                                                                           |
  |   '5' followed by '5948' returns the int from address 5948                                                                       |
  |                                                                                                                                  |
  |  6. writeStr [address] [inputString]                                                                                             |
  |   '6' followed by '345736' and then by 'Test String 1!' writes the String 'Test String 1! to address 345736                      |
  |                                                                                                                                  |
  |  7. readStr [address] [outputString]                                                                                             |
  |   '7' followed by '345736' reads the String from address 345736 into the outputString                                            |
  |                                                                                                                                  |
  |  8. writePage [page]                                                                                                             |
  |   '8' followed by '33' writes bytes from 0 to 255 sequentially to fill a page (256 bytes) starting with address 33               |
  |                                                                                                                                  |
  |  9. printPage [page]                                                                                                             |
  |   '9' followed by 33 reads & prints a page (256 bytes) starting with address 33. To just read a page to a data buffer, refer     |
  |    to 'ReadMe.md' in the library folder.                                                                                         |
  |                                                                                                                                  |
  |  10. printAllData                                                                                                                |
  |   '10' reads the entire chip and outputs the data as a byte array to the serial console                                          |
  |   This function is to extract data from a flash chip onto a computer as a text file.                                             |
  |   Refer to 'Read me.md' in the library for details.                                                                              |
  |                                                                                                                                  |
  |  11. Erase 4KB sector                                                                                                            |
  |   '11'  followed by 2 erases a 4KB sector containing the address be erased                                                       |
  |   Page 0-15 --> Sector 0; Page 16-31 --> Sector 1;......Page 4080-4095 --> Sector 255                                            |
  |                                                                                                                                  |
  |  12. Erase 32KB block                                                                                                            |
  |   '12'  followed by 2 erases a 32KB block containing the address to be erased                                                    |
  |   Page 0-15 --> Sector 0; Page 16-31 --> Sector 1;......Page 4080-4095 --> Sector 255                                            |
  |                                                                                                                                  |
  |  13. Erase 64KB block                                                                                                            |
  |   '13'  followed by 2 erases a 64KB block containing the address to be erased                                                    |
  |   Page 0-15 --> Sector 0; Page 16-31 --> Sector 1;......Page 4080-4095 --> Sector 255                                            |
  |                                                                                                                                  |
  |  14. Erase Chip                                                                                                                  |
  |   '14' erases the entire chip                                                                                                    |
  |                                                                                                                                  |
  ^----------------------------------------------------------------------------------------------------------------------------------^
*/
//#include <SPI.h>
#include<SPIMemory.h>
uint8_t pageBuffer[256];
String serialCommand;
char printBuffer[128];
uint32_t addr;
uint8_t dataByte;
uint16_t dataInt;
String inputString, outputString;

//Define a flash memory size (if using non-Winbond memory) according to the list in defines.h
//#define CHIPSIZE MB64

#if defined(ARDUINO_SAMD_ZERO) && defined(SERIAL_PORT_USBVIRTUAL)
// Required for Serial on Zero based boards
#define Serial SERIAL_PORT_USBVIRTUAL
#endif

#if defined (SIMBLEE)
#define BAUD_RATE 250000
#define RANDPIN 0
#else
#define BAUD_RATE 9600
#if defined(ARCH_STM32)
#define RANDPIN PA0
#else
#define RANDPIN A0
#endif
#endif
#define SS 3
//SPIFlash flash;                   
SPIFlash flash(SS, &SPI);       //Use this constructor if using an SPI bus other than the default SPI. Only works with chips with more than one hardware SPI bus

void setup() {
  
  Serial.begin(BAUD_RATE);
#if defined (ARDUINO_ARCH_SAMD) || (__AVR_ATmega32U4__) || defined(ARCH_STM32) || defined(NRF5)
  while (!Serial) ; // Wait for Serial monitor to open
#endif
  delay(250); //Time to terminal get connected
  Serial.print(F("Initialising"));
  for (uint8_t i = 0; i < 10; ++i)
  {
    Serial.print(F("."));
  }
  Serial.println();
  randomSeed(analogRead(RANDPIN));
  Serial.println("--------------");
 Serial.print("MOSI: ");
  Serial.println(MOSI);
  Serial.print("MISO: ");
  Serial.println(MISO);
  Serial.print("SCK: ");
  Serial.println(SCK);
  Serial.print("SS: ");
  Serial.println(SS);  
 Serial.println("--------------");
  flash.begin();
  //To use a custom flash memory size (if using memory from manufacturers not officially supported by the library) - declare a size variable according to the list in defines.h
  //flash.begin(MB(1));
  
  Serial.println();
  Serial.println();
  commandList();
}

void loop() {
  while (Serial.available() > 0) {
    uint8_t commandNo = Serial.parseInt();
    if (commandNo == 0) {
      commandList();
    }
    else if (commandNo == 1) {
      printLine();
      Serial.println(F("                                                      Function 1 : Get JEDEC ID                                                   "));
      printLine();
      printLine();
      uint8_t b1, b2, b3;
      uint32_t JEDEC = flash.getJEDECID();
      //uint16_t ManID = flash.getManID();
      b1 = (JEDEC >> 16);
      b2 = (JEDEC >> 8);
      b3 = (JEDEC >> 0);
      clearprintBuffer();
      sprintf(printBuffer, "Manufacturer ID: %02xh\nMemory Type: %02xh\nCapacity: %02xh", b1, b2, b3);
      Serial.println(printBuffer);
      clearprintBuffer();
      sprintf(printBuffer, "JEDEC ID: %04xh", JEDEC);
      Serial.println(printBuffer);
      printLine();
      printNextCMD();
    }
    else if (commandNo == 2) {
      printLine();
      Serial.println(F("                                                       Function 2 : Write Byte                                                    "));
      printSplash();
      printLine();
      inputAddress();
      Serial.print(F("Please enter the value of the byte (0-255) you wish to save: "));
      while (!Serial.available()) {
      }
      dataByte = Serial.parseInt();
      Serial.println(dataByte);
      if (flash.writeByte(addr, dataByte)) {
        clearprintBuffer();
        sprintf(printBuffer, "%d has been written to address %d", dataByte, addr);
        Serial.println(printBuffer);
      }
      else {
        writeFail();
      }
      printLine();
      printNextCMD();
    }
    else if (commandNo == 3) {
      printLine();
      Serial.println(F("                                                       Function 3 : Read Byte                                                     "));
      printSplash();
      printLine();
      inputAddress();
      clearprintBuffer();
      sprintf(printBuffer, "The byte at address %d is: ", addr);
      Serial.print(printBuffer);
      Serial.println(flash.readByte(addr));
      printLine();
      printNextCMD();
    }
    else if (commandNo == 4) {
      printLine();
      Serial.println(F("                                                       Function 4 : Write Word                                                    "));
      printSplash();
      printLine();
      inputAddress();
      Serial.print(F("Please enter the value of the word (>255) you wish to save: "));
      while (!Serial.available()) {
      }
      dataInt = Serial.parseInt();
      Serial.println(dataInt);
      if (flash.writeWord(addr, dataInt)) {
        clearprintBuffer();
        sprintf(printBuffer, "%d has been written to address %d", dataInt, addr);
        Serial.println(printBuffer);
      }
      else {
        writeFail();
      }
      printLine();
      printNextCMD();
    }
    else if (commandNo == 5) {
      printLine();
      Serial.println(F("                                                       Function 5 : Read Word                                                     "));
      printSplash();
      printLine();
      inputAddress();
      clearprintBuffer();
      sprintf(printBuffer, "The unsigned int at address %d is: ", addr);
      Serial.print(printBuffer);
      Serial.println(flash.readWord(addr));
      printLine();
      printNextCMD();
    }
    else if (commandNo == 6) {
      printLine();
      Serial.println(F("                                                      Function 6 : Write String                                                   "));
      printSplash();
      printLine();
      Serial.println(F("This function will write a String of your choice to the page selected."));
      inputAddress();
      Serial.println(F("Please enter the String you wish to save: "));
      while (!Serial.available()) {
      }
      readSerialStr(inputString);
      if (flash.writeStr(addr, inputString)) {
        clearprintBuffer();
        Serial.print(F("String '"));
        Serial.print(inputString);
        sprintf(printBuffer, "' has been written to address %d", addr);
        Serial.println(printBuffer);
      }
      else {
        writeFail();
      }
      printLine();
      printNextCMD();
    }
    else if (commandNo == 7) {
      printLine();
      Serial.println(F("                                                      Function 7 : Read String                                                    "));
      printSplash();
      printLine();
      Serial.print(F("This function will read a string from your address of choice: "));
      inputAddress();
      clearprintBuffer();
      sprintf(printBuffer, "The String at address %d is: ", addr);
      Serial.print(printBuffer);
      flash.readStr(addr, outputString);
      Serial.println(outputString);
      printLine();
      printNextCMD();
    }
    else if (commandNo == 8) {
      printLine();
      Serial.println(F("                                                       Function 8 : Write Page                                                    "));
      printSplash();
      printLine();
      Serial.println(F("This function will write a sequence of bytes (0-255) starting from your address of choice"));
      Serial.print(F("Please enter the address you wish to write to: "));
      while (!Serial.available()) {
      }
      addr = Serial.parseInt();
      Serial.println(addr);
      for (uint16_t i = 0; i < SPI_PAGESIZE; ++i) {
        pageBuffer[i] = i;
      }
      if (flash.writeByteArray(addr, &pageBuffer[0], SPI_PAGESIZE)) {
        clearprintBuffer();
        sprintf(printBuffer, "Values from 0 to 255 have been written starting from the address %d", addr);
        Serial.println(printBuffer);
        printReadChoice();
        while (!Serial.available()) {
        }
        uint8_t choice = Serial.parseInt();
        Serial.println(choice);
        if (choice == 1) {
          printOutputChoice();
          while (!Serial.available()) {
          }
          uint8_t outputType = Serial.parseInt();
          Serial.println(outputType);
          printPage(addr, outputType);
        }
      }
      else {
        writeFail();
      }
      printLine();
      printNextCMD();
    }
    else if (commandNo == 9) {
      printLine();
      Serial.println(F("                                                       Function 9 : Read Page                                                    "));
      printSplash();
      printLine();
      Serial.println(F("This function will read 256 bytes from the address selected."));
      Serial.print(F("Please enter the address you wish to read: "));
      while (!Serial.available()) {
      }
      addr = Serial.parseInt();
      Serial.println(addr);
      printOutputChoice();
      while (!Serial.available()) {
      }
      uint8_t outputType = Serial.parseInt();
      Serial.println(outputType);
      printPage(addr, outputType);
      printLine();
      printNextCMD();
    }
    else if (commandNo == 10) {
      printLine();
      Serial.println(F("                                                     Function 10 : Read All Pages                                                  "));
      printSplash();
      printLine();
      Serial.println(F("This function will read the entire flash memory."));
      Serial.println(F("This will take a long time and might result in memory issues. Do you wish to continue? (Y/N)"));
      char c;
      while (!Serial.available()) {
      }
      c = (char)Serial.read();
      if (c == 'Y' || c == 'y') {
        printOutputChoice();
        while (!Serial.available()) {
        }
        uint8_t outputType = Serial.parseInt();
        Serial.println(outputType);
        printAllPages(outputType);
      }
      printLine();
      printNextCMD();
    }
    else if (commandNo == 11) {
      printLine();
      Serial.println(F("                                                       Function 11 : Erase 4KB sector                                               "));
      printSplash();
      printLine();
      Serial.println(F("This function will erase a 4KB sector."));
      Serial.print(F("Please enter the address you wish to erase: "));
      while (!Serial.available()) {
      }
      addr = Serial.parseInt();
      Serial.println(addr);
      if (flash.eraseSector(addr)) {
        clearprintBuffer();
        sprintf(printBuffer, "A 4KB sector containing address %d has been erased", addr);
        Serial.println(printBuffer);
        printReadChoice();
        while (!Serial.available()) {
        }
        uint8_t choice = Serial.parseInt();
        Serial.println(choice);
        if (choice == 1) {
          printOutputChoice();
          while (!Serial.available()) {
          }
          uint8_t outputType = Serial.parseInt();
          Serial.println(outputType);
          printPage(addr, outputType);
        }
      } else {
        Serial.println("Erasing sector failed");
      }
      printLine();
      printNextCMD();
    }
    else if (commandNo == 12) {
      printLine();
      Serial.println(F("                                                       Function 12 : Erase 32KB Block                                              "));
      printSplash();
      printLine();
      Serial.println(F("This function will erase a 32KB block."));
      Serial.print(F("Please enter the address you wish to erase: "));
      while (!Serial.available()) {
      }
      addr = Serial.parseInt();
      Serial.println(addr);
      if (flash.eraseBlock32K(addr)) {
        clearprintBuffer();
        sprintf(printBuffer, "A 32KB block containing address %d has been erased", addr);
        Serial.println(printBuffer);
        printReadChoice();
        while (!Serial.available()) {
        }
        uint8_t choice = Serial.parseInt();
        Serial.println(choice);
        if (choice == 1) {
          printOutputChoice();
          while (!Serial.available()) {
          }
          uint8_t outputType = Serial.parseInt();
          Serial.println(outputType);
          printPage(addr, outputType);
        }
      } else {
        Serial.println("Erasing block 32K failed");
      }
      printLine();
      printNextCMD();
    }
    else if (commandNo == 13) {
      printLine();
      Serial.println(F("                                                       Function 13 : Erase 64KB Block                                              "));
      printSplash();
      printLine();
      Serial.println(F("This function will erase a 64KB block."));
      Serial.print(F("Please enter the address you wish to erase: "));
      while (!Serial.available()) {
      }
      addr = Serial.parseInt();
      Serial.println(addr);
      if (flash.eraseBlock64K(addr)) {
        clearprintBuffer();
        sprintf(printBuffer, "A 64KB block containing address %d has been erased", addr);
        Serial.println(printBuffer);
        printReadChoice();
        while (!Serial.available()) {
        }
        uint8_t choice = Serial.parseInt();
        Serial.println(choice);
        if (choice == 1) {
          printOutputChoice();
          while (!Serial.available()) {
          }
          uint8_t outputType = Serial.parseInt();
          Serial.println(outputType);
          printPage(addr, outputType);
        }
      } else {
        Serial.println("Erasing block 64K failed");
      }
      printLine();
      printNextCMD();
    }
    else if (commandNo == 14) {
      printLine();
      Serial.println(F("                                                      Function 14 : Erase Chip                                                    "));
      printSplash();
      printLine();
      Serial.println(F("This function will erase the entire flash memory."));
      Serial.println(F("Do you wish to continue? (Y/N)"));
      char c;
      while (!Serial.available()) {
      }
      c = (char)Serial.read();
      if (c == 'Y' || c == 'y') {
        if (flash.eraseChip())
          Serial.println(F("Chip erased"));
        else
          Serial.println(F("Error erasing chip"));
      }
      printLine();
      printNextCMD();
    }
  }
}

//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~Functions~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~//

void clearprintBuffer()
{
  for (uint8_t i = 0; i < 128; i++) {
    printBuffer[i] = 0;
  }
}

//Reads a string from Serial
bool readSerialStr(String &inputStr) {
  if (!Serial)
    Serial.begin(115200);
  while (Serial.available()) {
    inputStr = Serial.readStringUntil('\n');
    return true;
  }
  return false;
}

//Prints hex/dec formatted data from page reads - for debugging
void _printPageBytes(uint8_t *data_buffer, uint8_t outputType) {
  char buffer[10];
  for (int a = 0; a < 16; ++a) {
    for (int b = 0; b < 16; ++b) {
      if (outputType == 1) {
        sprintf(buffer, "%02x", data_buffer[a * 16 + b]);
        Serial.print(buffer);
      }
      else if (outputType == 2) {
        uint8_t x = data_buffer[a * 16 + b];
        if (x < 10) Serial.print("0");
        if (x < 100) Serial.print("0");
        Serial.print(x);
        Serial.print(',');
      }
    }
    Serial.println();
  }
}

//Reads a page of data and prints it to Serial stream. Make sure the sizeOf(uint8_t data_buffer[]) == 256.
void printPage(uint32_t _address, uint8_t outputType) {
  if (!Serial)
    Serial.begin(115200);

  char buffer[24];
  sprintf(buffer, "Reading address 0x(%04x)", _address);
  Serial.println(buffer);

  uint8_t data_buffer[SPI_PAGESIZE];
  flash.readByteArray(_address, &data_buffer[0], SPI_PAGESIZE);
  _printPageBytes(data_buffer, outputType);
}

//Reads all pages on Flash chip and dumps it to Serial stream.
//This function is useful when extracting data from a flash chip onto a computer as a text file.
void printAllPages(uint8_t outputType) {
  if (!Serial)
    Serial.begin(115200);

  Serial.println("Reading all pages");
  uint8_t data_buffer[256];

  uint32_t maxAddr = flash.getCapacity();
  for (int a = 0; a < maxAddr; a++) {
    flash.readByteArray(a, &data_buffer[0], 256);
    _printPageBytes(data_buffer, outputType);
    delay(100);
  }
}

//~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~Print commands~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~//

void printLine()
{
  Serial.println(F("----------------------------------------------------------------------------------------------------------------------------------"));
}

void printSplash()
{
  Serial.println(F("                                                        SPIFlash library test                                                     "));
}

void printNextCMD()
{
  Serial.println(F("Please type the next command. Type 0 to get the list of commands"));
}

void printOutputChoice()
{
  Serial.print("Would you like your output in decimal or hexadecimal? Please indicate with '1' for HEX or '2' for DEC: ");
}

void printReadChoice()
{
  Serial.print("Type 1 to read the page you have just modified. Type 0 to continue: ");
}

void writeSuccess()
{
  Serial.println("Data write successful");
}

void writeFail()
{
  Serial.println("Data write failed");
}

void inputAddress(void) {
  Serial.print(F("Please enter the address (0 - CAPACITY) you wish to access: "));
  while (!Serial.available()) {
  }
  addr = Serial.parseInt();
  Serial.println(addr);
}