XIAO RP2040 Schematic appears incomplete / outdated

Hi @Citric, there’s still a problem with the latest schematic - the RX LED and TX LED pin assignments are incorrect as per k_akiba’s post. I can confirm they are not on GPIO0 and GPIO1. Toggling GPIO16 and GPIO17 does blink them though, however v1.10 schematic has these as unassigned.

Edit: also noting that the board image on the wiki shows a red, green, and blue USER LEDs instead of 2 blue LEDs for RX and TX, which seems to be correct for my XIAORP2040 boards but disagrees with this schematic still

1 Like