XIAO RP2040 Schematic appears incomplete / outdated

The LED part of the V1.0 circuit diagram is also strange.
On the board I got
The red LED of Tx is GPIO17
Rx green LED is GPIO16
Is connected to.
In the V1.0 schematic, the Eagle PCB is also different from the actual one, and Tx is directly connected to GPIO0.

Perhaps the design was changed along the way.

1 Like