XIAO Round Display Not Detecting SD Card

I tried that, and got compiler errors, indicating the pins are already defined.
Tried going to the pin definition file, changed the pin number, but unfortunately no dice.

I also tried just copy/paste the pinout you provided, and while it still compiled, I get zero output now.

I tried just changing the SS pins to 28, but also no luck.

It seems it has two different SPI_SS pins defined, but it’s labeled as not pinned out:
#define PIN_SPI0_SS (31u) // not pinned out

// Not pinned out
#define PIN_SPI1_MISO  (31u)
#define PIN_SPI1_MOSI  (31u)
#define PIN_SPI1_SCK   (31u)
#define PIN_SPI1_SS    (28u)