XIAO Round Display Not Detecting SD Card

Hi there,
Ok so, Then…
Those are almost correct, for an Xiao RP2040

I would do something like this.* #define SS 28
first then go all in.
Try that?

// Map SPI port to 'new' pins
#define PIN_SPI_SS    (28)
#define PIN_SPI_MOSI  (3)
#define PIN_SPI_MISO  (4)
#define PIN_SPI_SCK   (2)

static const uint8_t SS   = PIN_SPI_SS;
static const uint8_t MOSI = PIN_SPI_MOSI;
static const uint8_t MISO = PIN_SPI_MISO;
static const uint8_t SCK  = PIN_SPI_SCK;

For grins , Try the Name of pin as well, i.e. A2,D10,D9, D7
HTH
GL :slight_smile: PJ