Xiao nrf52840 Sense: BLE connection is lost during delay()

HI there,
So I tweaked it and Tested with NRF connect BLE ver 4.04 seems to stay connected and doesn’t output anything until I move it, then prints paused until idle(at rest) BLE stay’s connected AOK.
Here is output from NFR connect BLE desktop

#include <ArduinoBLE.h>
#include <Arduino.h>
#include <LSM6DS3.h>
#include <Wire.h>

//Create a instance of class LSM6DS3
LSM6DS3 myIMU(I2C_MODE, 0x6A);  //I2C device address 0x6A
const char* UUID_serv = "75681d64-fd7e-40f7-874f-c6f2e7ec996c";

// UUids for accelerometer characteristics
const char* UUID_AccBLE = "75681d64-dd7e-40f7-874f-c6f2e7ec996c";

BLEService myService(UUID_serv);
BLEIntCharacteristic AccBLE(UUID_AccBLE, BLERead | BLENotify);

void setup() {
  // put your setup code here, to run once:
  Serial.begin(9600);
  Serial.println("Power ON ");  // Let's BEGIN!!
  Serial.println("Test program compiled on " __DATE__ " at "__TIME__);
  Serial.println();
  myIMU.settings.gyroEnabled = 0;  // Gyro currently not used, disabled to save power
  while (!Serial) {

    //Call .begin() to configure the IMUs
    if (myIMU.begin() != 0) {
      Serial.println("Device error");
    } else {
      Serial.println("Device OK!");
    }
    // init BLE
    if (!BLE.begin()) {
      Serial.println("BLE: failed");
    }
    setupblink();        // Tests The onboard RGB LED
    Serial.println("BLE: ok");
    BLE.setLocalName("BLUE ACCEL");
    BLE.setDeviceName("BLUE ACCEL");    
    BLE.setAdvertisedService(myService);
    myService.addCharacteristic(AccBLE);
    BLE.addService(myService);
    AccBLE.writeValue(0);
    // start advertising
    BLE.advertise();
    Serial.println("Advertising started");
    Serial.println("Bluetooth device active, waiting for connections...");
  }
}
float accelerometerX;
unsigned long BreakPreviousMillis;

int x_time = 4000;// 400000
void loop() {
  BLEDevice central = BLE.central();
  if (central) {
    Serial.print("Connected to central: ");


    while (central.connected()) {
      accelerometerX = myIMU.readFloatAccelX();
      if (accelerometerX > 2) {
        BreakPreviousMillis = millis();
        while (millis() < BreakPreviousMillis + x_time) {
          Serial.println("pause");
        }
      Serial.println("run");
      }

      AccBLE.writeValue(accelerometerX);
    }

    digitalWrite(LEDB, HIGH);  // High == turning off the Led
    Serial.print("Disconnected from central: ");
    Serial.println(central.address());
  }
}

void setupblink() {
  pinMode(LEDR, OUTPUT);  // initialize the LED pin as an output:
  pinMode(LEDG, OUTPUT);  // initialize the LED pin as an output:
  pinMode(LEDB, OUTPUT);
  pinMode(LED_BUILTIN, OUTPUT);  // initialize the LED pin as an output:
  setLedRGB(false, true, false);  // Red
  delay(1000);
  setLedRGB(true, false, false);  // Green
  delay(1000);
  setLedRGB(false, false, true);  // Blue
  delay(1000);
  setLedRGB(false, false, false);  // OFF
}

void setLedRGB(bool red, bool green, bool blue) {

  if (!blue) {
    digitalWrite(LEDB, HIGH);
  } else {
    digitalWrite(LEDB, LOW);
  }
  if (!green) {
    digitalWrite(LEDG, HIGH);
  } else {
    digitalWrite(LEDG, LOW);
  }
  if (!red) {
    digitalWrite(LEDR, HIGH);
  } else {
    digitalWrite(LEDR, LOW);
  }
}



Stays connected until I disconnect ,see pic and the word “run” BLE is still connected and will disconnect and reconnect AOK.

HTH
GL:-)