XIAO nrf52840 PLUS documentation has incorrect pinouts!

I’ve burnt a whole day trying to diagnose things. Finally did a sanity check checking if each pin actually was right. Found that the documentation is wrong.

The image that shows the new pins for the xiao nrf52840 plus is wrong.
1.03 and 1.07 are SWAPPED.
I’ve confirmed this with the kicad files.
It looks like it’s only these two pins.

I hope this saves people the hours of troubleshooting it could cause.

Sincerely a far more bald individual

Hi there,

and welcome back…here.
So cool you even got one, I’m waiting still.
Ah’ the pain of early adopters, we suffer in silence until now
:grin::v:

good catch btw, I’m of the opinion they should have developed the connectivity first. socket, or edge connector dense enough to support those extra castilations… :stuck_out_tongue_closed_eyes:
I’ll have a video of the innovative test socket(Xiao Clip Base) coming up soon.


HTH
GL :slight_smile: PJ :v:

Hi Alakuu,

Indeed there is a inconsistent in the KiCAD file and PCB schematic as you suggested, we’ll fix this issue.

We appreciate your feedback!

1 Like

I think this is still not correct.

Which Arduino port-number corresponds to f.e. P1.01? It’s not D13!

So what I found out, P1.13 is 37, P1.14 is 38…

Hi,
Thank you for your feedback. We have reported the issue to the relevant personnel, and will update here once we have the latest conclusions.

Best Regards!

Hi,
Sorry I’m late.
You can download the PCB schematic and KICAD files from the wiki. After comparing them, I found that they are consistent.
https://files.seeedstudio.com/wiki/XIAO-BLE/Seeed_Studio_XIAO_nRF52840_Plus_SCH_PCB_v1.1.zip
https://files.seeedstudio.com/wiki/XIAO-BLE/Seeed_Studio_XlAO_nRF52840_Plus_KiCAD_file.zip

What do you mean by 37 and 38?
Looking forward to your reply