I am using tools to simply read the tag, hoping that it will read hello world. I cannot post any images (i think because i am new user) but it is pretty much identical to the molex/seeed nrf image posted by adriandreo above. Short equal length wires soldered to both the antenna and the nfc terminals. I am using Arduino IDE to compile and flash, here is the output. WARNING: library NFC claims to run on nrf52 architecture(s) and may be incompatible with your current board which runs on mbed architecture(s).
Sketch uses 87536 bytes (10%) of program storage space. Maximum is 811008 bytes.
Global variables use 44384 bytes (18%) of dynamic memory, leaving 193184 bytes for local variables. Maximum is 237568 bytes.
Upgrading target on /dev/cu.usbmodem14301 with DFU package /Users/elliottlambertparsons/Library/Caches/arduino/sketches/52386E8CE59F93C3083B72C146E7A7F8/sketch_mar11a.ino.zip. Flow control is disabled, Single bank, Touch disabled
########################################
########################################
########################################
########################################
###########
Activating new firmware
Device programmed.