XIAO nRF52840 NFC Antenna Insights

Hi there,

Yes, It’s divided in Half to get the actual Values.
I use the DeV Board with the Factory ant in previous picture.

HTH
GL :slight_smile: PJ :v:

fyi:
Nordic specifies that two capacitors (one per NFC pad) should each be half of the total capacitance.

Thus, for 2.6 µH, each capacitor should be:

Ceach=Ctotal2=20.32=10.15 pFC_{\text{each}} = \frac{C_{\text{total}}}{2} = \frac{20.3}{2} = 10.15 \text{ pF}Ceach​=2Ctotal​​=220.3​=10.15 pF