XIAO nRF52840 NFC Antenna Insights

Hi there,

Ok so that’s the full monty , but I see you are using the 2.9.3 BSP
The wiki was a 2.9.2 so I would first start by rolling that back and try again. I recommend try just the non embed too, 1.1.3 BSP.
or /then
Post up a picture so we can check it over. :+1:
and the Whole code you are using or just the wiki?
NOTE:
WHAT is the Inductance of the -0001 version ?
If it’s not exact then IT won’t work.
If you used 43pf tunning caps, and a different Molex Ant. IT won’t work.

If you look at the OP data sheets for both antennas for example they list the Micro-Henries of the respective devices at the resonant frequency of 13.56Mhz
I couldn’t find the spec on yours. -0001


you use it in the equazion and add the appropriate tuning values,

HTH
GL :slight_smile: PJ :v: