Xiao MG24 Sense onboard gyroscope

Hi there,

So just as a test, I went external and connected a grove IMU Sure enough it works this way… LOL :face_with_peeking_eye: My guess is it will need a different LIB, I get an SPI divide clock error with the other Arduino or Seeed LIB :face_vomiting: :-1: so far I’m NOT a FAN of SIL…
Also I see the power IMU is on pin PD05 , Do we need to turn this ON to get it to work maybe? an Extra Step?

HTH
GL :slight_smile: PJ :v:

I don’t like there is NO interrupt PIN connected either in the Schematic for this Bomb.
at Least the Xiao Nrf52840 Sense has THAT! :sweat_smile: