XIAO MG24 Sense Low Power Library weirdness

Hi there,

Yea, @msfujino is also looking into it, appears that maybe different methods are required for the different levels of Sleep. Hmmm :face_with_peeking_eye:
Just because I like hearing myself; I would have checked if this device meets the minimum requirements in any New Xiao’s today.

  • Battery Monitor

  • Interrupts

  • Sleep modes

  • RTC

Then get cute with Peripherals, FastSPI, CAN bus, Dual Radio’s (concurrent)
i3C , WiF6, 5G , IOT.
Then have the Stacks or SD’s to back it… Zigbee, Thread, Matter, 4Mb PHY…
:star_struck: Someone kick me I’m dreaming…LOL

Anyway, expect the weirdness to continue Until we get the full 411 on this thing, until then for that reason , Like M Cuban "I’m Out "