XIAO looses its Ports

C:\XIAO_bootloader>
C:\XIAO_bootloader>C:\OpenOCD\OpenOCD-20211118-0.11.0\bin\openocd -f XIAO_openocd.cfg
Open On-Chip Debugger 0.11.0 (2021-11-18) [https://github.com/sysprogs/openocd]
Licensed under GNU GPL v2
libusb1 09e75e98b4d9ea7909e8837b7a3f00dda4589dc3
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
DEPRECATED! use ‘adapter srst delay’ not ‘adapter_nsrst_delay’
DEPRECATED! use ‘adapter srst pulse_width’ not ‘adapter_nsrst_assert_width’
Info : clock speed 400 kHz
Info : STLINK V2J17S4 (API v2) VID:PID 0483:3748
Info : Target voltage: 3.114796
Info : at91samd21g18.cpu: Cortex-M0+ r0p1 processor detected
Info : at91samd21g18.cpu: target has 4 breakpoints, 2 watchpoints
Info : starting gdb server for at91samd21g18.cpu on 3333
Info : Listening on port 3333 for gdb connections
target halted due to debug-request, current mode: Thread
xPSR: 0x81000000 pc: 0x00000288 msp: 0x20002dd8
target halted due to debug-request, current mode: Thread
xPSR: 0x81000000 pc: 0x00000288 msp: 0x20002dd8
** Programming Started **
Info : SAMD MCU: SAMD21G18A (256KB Flash, 32KB RAM)
Error: SAMD: NVM programming error
Error: Failed to erase row containing 00000000
Error: SAMD: failed to erase sector 0 at 0x00000000
Error: failed erasing sectors 0 to 31
embedded:startup.tcl:1029: Error: ** Programming Failed **
in procedure ‘script’
at file “embedded:startup.tcl”, line 26
in procedure ‘program’ called at file “XIAO_openocd.cfg”, line 20
in procedure ‘program_error’ called at file “embedded:startup.tcl”, line 1094
at file “embedded:startup.tcl”, line 1029

C:\XIAO_bootloader>